This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: LMK04832

Part Number: LMK04832

HI,

We are using LMK04832 in our designs.

Attached the schematics below.

Input is 100M TCXO. Outputs are 20MHz CMOS outputs.
We have configured all the outputs, But we are not getting any output from clkout 10 and 11. even if we enable both inverting and non inverting inputs, output is not coming on both pins.

The output of 10 and 11 is connected to a FPGA clock input PIN.
And the clockout12 is connected to the same pin of a second FPGA, and that output is coming properly.
Remaining 6 outputs are connected to different clock buffer and all are coming properly.

We have tried with two different boards and both behaves same.

Can you please suggest why LMK is behaving like this?

Best Regards,
Shafeeq