Part Number: LMK03328
Hi Team,
I tried eeprom programing using TICS pro GUI as well as by use of external I2C master, as mentioned programing method in datasheet of LMK03328 page no 56, but looks like it is not programming the epprom.
Below are the GPIO strapping settings,
REFSEL = High, primary clock 100MHz input
HW_SW_CNTL = low, Soft pin mode
GPIO0 = high, o/p sync
GPIO1 = Low, i2c address ix 0x54
GPIO2-3 = Low, EEPROM page 0 loading
GPIO4 = High, Soft pin mode
GPIO5 = float
I am able to program its registers via external i2c master and I am able to get desired output frequency on channel 0.
Observed that, Once SRAM write and EEPROM write procedure completed, no increment at R136 value.