Part Number: LMK05028
Other Parts Discussed in Thread: LMK05318B, LMK5B33414, LMK5B33216, LMK5B12204
Hi,
I'm using the LMK05028 to synchronize to a 1PPS input and generate a 1PPS, 32.768MHz & 2.56KHz at the outputs using only DPLL2. The outputs need to be phase aligned to the 1PPS clock input. Im having trouble reliably validating my 1PPS input and getting the DPLL to lock in this configuration, both frequency and phase.
When my 1PPS input does get validated it seems reliable but still unable to get the DPLL to lock
Sometimes the device struggles to validate the 1PPS input also.
My TICS pro file is: MDAQ_LMK05028_1PPS_HI_CS_2.56KHZ_R1.tcs
I have tried suggestions made in this forum for this device, but I cannot get the frequency and the phase to lock after successful reference validation.
I am using:
FT3HNBPK10.0-T1 as my 10MHz input source
Quectel L26T-S89 for my 1PPS source and this is validated. Its duty cycle is 50%
Other threads indicate this device may not be suitable for use with 1PPS inputs ad the alternate devices suggested are not suitable for my requirements. Do you have any suggestions i can try with this chip?