Part Number: LMK04828
Other Parts Discussed in Thread: LMK04832, LMK04821, LMK04826, LMK04228
According to the TI spec sheet, the LMK04828 uses a 24-bit SPI transaction length. Can I drive the LMK04828 SPI interface with a 32-bit SPI word and shift the 24-bit "word of interest" such that the first 8-bits shifted in are zeroes? Since the LMK04828 basically clocks the SPI bits into a shift register, assuming it's a 24-bit shift register, will it keep shifting the full 32-bits in and keep the last 24-bits prior to the CS being deasserted?
Any clarifications would be very helpful.
Best regards,
David