This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My customer has questions about “Single-Event Effects Test Report for CDCLVP111-SP 1:10 LVPECL Clock Distributor”
Q1:
On the Figure10 on page 13, which output are measured, Q0, Q9 or total Q0 and Q9?
Q2:
To estimate total 10 outputs (Q0 – Q9) Weibull FIT, will the result be 5x Figure10 or 10x Figure10?
Best regards,
K.Hirano
I found the data that was used to create the report and it appears that figure 10 is for Q0 only.
As shown in the report, 45% of the time there was an event on Q0 there was also one on Q9. I would agree that the total number of unique events might be 5x of that measured on one output.