The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05028: LMK05028: How to use GPS PPS as the reference clock to generate 40 MHz

Part Number: LMK05028
Other Parts Discussed in Thread: SN74AXC8T245EVM, LMK5C33216, LMK5B33216

Hello,

I try to follow the test in the forum :"LMK05028: How to use GPS PPS as the reference clock to prevent output frequency drift?"

LMK05028: How to use GPS PPS as the reference clock to prevent output frequency drift? - Clock & timing forum - Clock & timing - TI E2E support forums

Bellow is my test:

- Configuration load : LMK05028_1PPS_config_40MHz_out_onboard_XO_and_TCXO_V2.tcs, I use the EVM.

- Input PPS : connected IN0_P, 1V8, Duty cycle 50%. The signal is OK in the oscilloscope. IN0_N is connected to 50 ohm cap.

For my test, I use an EVK-M8T GNSS Evaluation Kit (EVK-M8T). I configure the PPS to have a Duty cycle 50% instead of 10%, 3V3. I use an SN74AXC8T245EVM (TI) for having 1V8. The EVK-M8T GNSS is connected to the GNSS ANTENNA.*

I follow this procedure (from Kia Rahbar):

1. Load the above configuration.

2. Press a soft-reset chip.

3. Readback your status registers.

- It will take about 5-10 seconds for the reference to validate (REF0VALSTAT to go high), about 5-10 seconds for the HLDOVR1 flag to go low, about 20-25 seconds for the LOFL_DPLL1 flag to go low, => That is OK 

- about 2-3 minutes for the LOPL_DPLL1 flag to go low.  => LOPL_DPLL1 flag is always high

Results : 

- I have 40.0014 MHz,

- I have frequency drift,

- Always LOPL_DPLL1 high

My questions is what do you use for generating the Input PPS connected to IN0_P to have LOPL_DPLL1 low?

Thank you,

Patrice