Part Number: LMK1C1108
I have a design with 1.8V supply where the input is a 25MHz clipped sine. The V_IL, V_IH and the negative slew rate are within specification but the positive slew rate is just outside with 0.07 V/ns. It seems to work nicely anyway so I wonder what is the potential effect or risk of this? We are for example limited to a temperature span of -40C to + 85C.