Part Number: LMX2594
Hi there!!
I am using LMX2594 and want to use a sync mode.
I have set the PLL as the pic below

There is a problem I want to fix.
When I set fractional mode which is the output of PLL is not a multiple of Fosc,
(For example Fosc : 100 MHz, Output : 4050Mhz)
The output of PLL looks like there is a fractional spur like below

And It doesn't happen If I use integer mode which is the output of PLL is a mutilication of Fosc.
(For example Fosc : 100 MHz, Output : 4000Mhz)
It looks very clean like below.

This issue specifically occurs only when in sync mode. (when VCO_Phase_Sync = 1)
Anyone know about this problem or how to fix?
Thanks