Part Number: CDCM61001
I am using the CDCM61001 IC and generate the LVDS differential ouput signal and give to Microprocessor.
Opearting voltage of (Driver)CDCM61001 is 3.3V and Used (Receiver)microprocessor's VDD=0.9V and VDDQ=1.5V
As mentioned in datasheet of CDCM61001, If the supply voltage of the driver and the receiver are different, ac-coupling(LVDS Output AC termination) is required.
I have no idea which termination is required. If i used LVDS Output AC termination than what is the value of capacitor in differential line(How to calculate capacitor value?