Part Number: LMX2592
Other Parts Discussed in Thread: LMX2594
Hi team,
i'm using the LMX2592 for the new project.
I have to jump between 2 frequencies from 4.95 GHz to 7.15 GHz with the minimum lock time.
I attach the register map for the 2 frequencies.
Which registers need to be modified to jump quickly?
Is there a workflow to follow similar to the full assist of the LMX2594? (see the application note SNAA336A).
Thank you in advance.
Best regards,
Matteo Ricci
R70 0x460000 R69 0x450000 R68 0x440089 R64 0x400077 R62 0x3E0000 R61 0x3D0001 R59 0x3B0000 R48 0x3003FD R47 0x2F08C4 R46 0x2E0423 R45 0x2D0000 R44 0x2C0000 R43 0x2B0000 R42 0x2A0000 R41 0x2903E8 R40 0x280000 R39 0x278204 R38 0x2600C6 R37 0x254000 R36 0x240011 R35 0x23021F R34 0x22C3EA R33 0x212A0A R32 0x20210A R31 0x1F0001 R30 0x1E0034 R29 0x1D0084 R28 0x1C2924 R25 0x190000 R24 0x180509 R23 0x178842 R22 0x162300 R20 0x14012C R19 0x130965 R14 0x0E018C R13 0x0D4000 R12 0x0C7001 R11 0x0B0018 R10 0x0A10D8 R9 0x090302 R8 0x081084 R7 0x0728B2 R4 0x041943 R2 0x020500 R1 0x010808 R0 0x00221C
R70 0x460000 R69 0x450000 R68 0x440089 R64 0x400077 R62 0x3E0000 R61 0x3D0001 R59 0x3B0000 R48 0x3003FD R47 0x2F08D3 R46 0x2E1323 R45 0x2D01F4 R44 0x2C0000 R43 0x2B0000 R42 0x2A0000 R41 0x2903E8 R40 0x280000 R39 0x278204 R38 0x26008E R37 0x255000 R36 0x240011 R35 0x23021F R34 0x22C3EA R33 0x212A0A R32 0x20210A R31 0x1F0001 R30 0x1E0035 R29 0x1D0084 R28 0x1C2924 R25 0x190000 R24 0x180509 R23 0x178842 R22 0x162300 R20 0x14012C R19 0x130965 R14 0x0E018C R13 0x0D4000 R12 0x0C7001 R11 0x0B0018 R10 0x0A10D8 R9 0x090302 R8 0x081084 R7 0x0728B2 R4 0x041943 R2 0x020500 R1 0x010808 R0 0x00221C