Part Number: CDCI6214
Other Parts Discussed in Thread: , CDCE6214, USB2ANY
Tool/software:
Hi expert,
Hardware platform:J721EXSOMG01EVM + J721EXCP01EVM
Software:ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05
1. The hardware schematic show EEPROMSEL pin pullup to high, as CDCI6214 manual document show the address should be 0x77, but can't find 0x77(find 0x76), why 0x76?



2. what should I do to generate 156.25MHz at Y3?
3. 

Are arrows 1 and 2 pointing to the same address?
4. 
Can I use i2c-tool to read the register 0x18?
Thanks a lot.
Best Regards!