This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK1D2102: LMK1D2102R - 50 Ohm Sine wave input support

Part Number: LMK1D2102


Tool/software:

Dear Team,

               We are  searching for the Fanout Buffer (10 MHz) which accepts the Single Ended 50 Ohm Sine Wave Input OCXO and covert it to square wave LVDS reference clock.

We are planning to use the LVDS buffer LMK1D2102R for this purpose.

1) Please clarify that, LMK1D2102R can be used for receiving Single Ended 50 Ohm Sine Wave Input ?

2) If fanout buffer supports this Single Ended 50 Ohm Sine Wave input then what is the recommended input clock termination?

Regards,

Esakki.