Part Number: LMK04832
Other Parts Discussed in Thread: LMK04828
Tool/software:
We have a LMK04832 on the board and like to get all clock outputs aligned between LMK04832 (or boards).
1. LMK04832 can be in single loop or single loop 0-delay mode.
2. CLKin1 is used as REF IN (not OSCin).
3. The phase aligned 100MHz reference clock and SYNC signals (aligned) are provided to each LMK04832 or board.
4. SYSREF outputs are continuous and programmable.
5. DCLK outputs are programmable.
see attached TICS Pro settings.
Question #1
Which one is better to get multiple LMK04832, 0-delay or not?
Question #2
Is SYNC signal (pin) required? in these two modes?
Question #3
I could not get the outputs aligned all the time.
Any suggestions? Thank you.