Other Parts Discussed in Thread: LMK04828
Tool/software:
Hi,
In our ZCU208 design, we need to generate DAC data using the SFP recovered clock from the PCS/PMA Ethernet. We're attempting to generate the DAC reference clock by programming the CLK104 RF Clock Add-on Card through TICSPRO. We're operating in dual loop mode and providing our SFP Rx recovered clock (62.5 MHz) as clkin2 input for the LMK04828B (U2). We are getting the DAC ref clk out signal but PLL1 in the LMK04828B is not locking. We've confirmed this by programming register R366 (0X016E1B address) to check the PLL1 lock status using the DS1 LED, which is blinking.
Interestingly, when we test with an oscillator input instead of the recovered clock, PLL1 locks successfully.
I am attaching the relevant TICSPRO configuration and clk104 block diagram as specified in UG1437.
Could you advise on how to ensure PLL1 locks when using SFP recovered clock as the input ? Also, could you clarify whether the SFP recovered clock input should be in CLKIN2 or CLKIN0? The documentation isn't very clear on this point.
Thank you