This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC555: his simulation file can only simulate 0-400 us,because of TLC555

Part Number: TLC555

Tool/software:

 final -20241119-4.TSC

This simulation file can only simulate 0-400 us, and an error message of U12 occurs when more time is added. What is the problem? How can it be solved so that the simulation can be extended to 30 ms or more? Otherwise, we cannot see the complete waveform.

I have set it up according to the instructions in the picture, but it still doesn't work.