Part Number: LMK05318BEVM
Tool/software:
Hi !
The precedent thread has been locked so I continue here.
I've got a 1Hz signal (this is the GPS' synchronization PPS) that arrives in the LMK05318BEVM.
I would like to have this same signal coming out of the LMK05318BEVM (synchronized in frequency and phase with the input one) when everything is fine and if I stop the input signal (for a long time, like one or two days), I would like the output signal to continue as if the input signal had never stopped, still synchronized in frequency and phase with the one that stopped.
I did something on TICSPRO that you'll find here :
2024-12-09_CONFIG_LMK05318B EVM_1PPS.tcs
When we look to the status, it seems that the component don't detect the input signal.
Can you give me a fonctionnal TICSPRO file that works with the evalboard LMK05318BEVM please ?
Thank you,
Have a nice day,
Coline