This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00334-Q1: Unused input tie off

Part Number: LMK00334-Q1


Tool/software:

If we are using the part as a 1:4 buffer and not using the muxing capability should I ground both sides of RX1 plus OSCin?

Also the part datasheet does not mention operation with spread spectrum.  My intention is to use as a buffer - accepting PCIe clock in and buffering to multiple devices plus a switch.  It mentioned PCIe Gen1-5 so I would assume yes but would be nice to confirm.

thanks.

Keith

  • Hello Keith, 

    If OSCin is not used pin can be grounded via 1kOhm PD resistors. 

    I believe you're asking if we can support SSC clocking - the answers is yes. 
    If the ref clk has SSC so will the outputs but the LMK0334 cannot output SSC outputs if the ref clk does not have SSC. 


    Best regards, 

    Vicente