Other Parts Discussed in Thread: LMK04616, LMK04616EVM
Tool/software:
Is this really the total power I can expect the LMK04610 to consume with Bypass mode turned on (no PLL1 or PLL2) for this configuration? I arrived at these numbers using table 226. Also, what is the additive Jitter when in Bypass PLLs mode?
| (mW) | ||
| CLKinX | Single-Ended Mode | 2.16 |
| SYSREF | Continuous Mode | 0 |
| Output 1 | HSDS 8mA | 16.2 |
| Output 2 | HSDS 8mA | 16.2 |
| Output 3 | HSDS 8mA | 16.2 |
| Output 4 | HSDS 8mA | 16.2 |
| Output 5 | HSDS 4mA | 9 |
| Output 6 | HSDS 4mA | 9 |
| Total Power (mW) | 84.96 |