Part Number: LMK04828
Other Parts Discussed in Thread: LMX2594
Tool/software:
We are working on ZCU208 board. We need to generate 1.96416GHz sampling rate with external clock 10.23MHz to CLK104 module consisting of LMK04828B.
I did configuration in TICs pro to generate 245.52MHz with CLKIn0 as 10.23MHz input (external reference input is coming through CLKin0 as per CLK104 data sheet).
The following configuration works even if I don't feed external 10.23MHz to CLK104. This will be working with internal VCOs and may not be generating 1.96416GHz sampling rate accurately. (This I'm confirming from external output of CLK104 which is SDCLKOUT11 of LMK, this should come 7.6725MHZ as per the configuration, but I'm getting 7.5MHz in oscilloscope).
One more thing what I observed is if I feed external clock 10.23MHz, CLK104 module PLL doesn't lock (This I'm observing in DS1 LED of CLK104). It gets locked only if 10MHz clock is fed with the above TICs pro configuration of 10.23MHz.
Kindly let me know whether the CLk104 module works for external 10.23MHz reference clock.
Or is there any way to achieve the desired sampling rate 1.96416GHz with 10MHz internal oscillator.
Screenshots of TICsPro configuration is attached.


regards
Salman