Other Parts Discussed in Thread: LMK04832
Tool/software:
Question: what is the LMX2820 output jitter degradation if I have a rather low pfd frequency such as 10_MHz?
For contrasting examples, the two examples below have similar VCO & output frequencies but substantially different pfd frequencies;
i.e. f_pfd= 10_MHz vs 320_MHz.
Two questions:
a. is there is a curve showing jitter degradation vs f_pdf around the region of f_pfd=10MHz?
b. is there is a curve showing the jitter degradation versus loop bandwidth with a low f_pfd frequency such as 10MHz?
EXAMPLE_1:
input = 640MHz
PFD = 10MHz
VCO = 10070MHz
output = 2517.5MHz
input_divider = 64
feedback_divider= 1007
output_divider = 4
f_out = 640 /64 * 1007 /4= 2517.5 MHz
f_pfd = 10070 / 1007 = 10 MHz
EXAMPLE_2:
input = 640_MHz
PFD = 320_MHz
VCO = 10240_MHz
output = 2560_MHz
input_divider = 2
feedback_divider= 32
output_divider = 4
f_out = 640 /2 * 32 /4= 2560_MHz
f_pfd = 10240 / 32 = 320_MHz
- samuel.stewart@ngc.com