Part Number: LMK04832
Tool/software:
Hello team,
I have questions about register information of LMK04832 below. Could you please give me comments?
- 0x162 Register
- OSCin_FREQ is different between Table 5 and Table 69. Table 69 says [4:2] while table 5 says [3:2].
In addition to this, when set 255MHZ < OSCin in TICS Pro, it shows 3 which is reserved according to Table 69.
Could you let me know correct information for this register field? - There is PLL2_XTAL_EN register field in Table 5, but the field is treated as reserved bit in Table 69.
Should we consider it as reserved bit like Table 69?
- 0x103, 0x10B, 0x113, 0x11B, 0x123, 0x12B, 0x133 Registers
in Table 21, field name of bit4 is CLKoutX_Y_PD but Table 5 says DCLKX_Y_PD in the field.
Right information is DCLKX_Y_PD, correct?
- 0x16E Register
There is no 0x16E register in Table 5.
Is it correct that 0x16E which is described in Table 77 should be in Table 5 instead of 0x16C?
Best regards,