Tool/software:
Hello team,
I have questions about register information of LMK04832 below. Could you please give me comments?
Best regards,
Hello Taketo-san,
1. OSCin_FREQ is 0x162 and should be bits R354[3:2].
Setting to 3 is 256MHz < Oscin
In TICSpro it's not reserved.
The register is linked to only bits 3&2 which indicates a DS mismatch.
In table 5 it does match but not in table 69 as you stated.
2.
This bit doesn't exist in TICSpro either.
Not sure why it's mentioned.
i would treat it as reserved.
3. You're correct - it should be DCLKX_Y_PD.
4. Correct.
Best regards,
Vicente
Hello Vicente-san,
Thanks for the comment.
Could you please fix these wrong information in datasheet to correct information in next revise timing?
Best regards,
Hello Taketo-san,
We will be sure to add this into the next datasheet update.
Thanks,
Michael