This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: Output Clocks Not Phase Aligned with Input Clock in 0-delay Mode

Part Number: LMK04832

Tool/software:

Hi All,

Utilizing an LMK04832 we are attempting to edge align the CLKout, External VCXO (OscIn for PLL2), and ClkInX. After reading the datasheet, we believe 0-delay is the best method to get this done. We have attempted to set the PLL into dual-loop 0-delay nested + cascaded without any luck. 

We have attached our TICS PRO configuration in case we are missing a config. We have measured a 30ns offset between ClkInX (10MHz) and ClkOut (10MHz). We are aware that in 0-delay mode, there is a deterministic phase relationship with VCXO, ClkIn, and output Clocks and they may not be edge aligned.

We are looking for a sync, PLL R divider sync, or offset we can apply to edge align our ClkInX, OscIn, and ClkOut. 

Thank you for the assistance,

Grant

LMK04832_NC_IDL_ODL.tcs