This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: LMX2595EVM Manual Ramping mode

Part Number: LMX2595


Tool/software:

Hi there,

I have a problem with manual ramping mode with LMX2595EVM.

Could you please help me with it?

LMX2595EVM has been set up as below

LMX2595EVM setting

Fosc: 125MHz, R: 5, FPD: 25, RFoutA: 14000MHz

Manaul Ramping Mode

       

RAMP0: 25MHz -> RAMP1: -25MHz -> Clicked 'Update Ramp GUI' -> checked 'RAMP_EN' -> clicked 'Clock Ramp'

or Update Ramp GUI-> Clock Ramp -> RAMP_EN

or Clock Ramp->Update Ramp GUI->RAMP_EN

or other orders

Tried several ways and times to do ramping; however, manual ramping is not working at all...

Back to PPL to check Fractional denominator is 4294967295

When I check RAMPDIR and RAMPCLK TPs with ocillator, there are no signals...

I checked that the harware has RampClk and RampDir connected to the device.

As you know that sv601349 has been used to control the PLL.

  

U2A_GPIO7 -> RampDIR & U2A_GPIO3 -> RampClk_TP

When I click the 'Clock Ramp', there are no signals from RampDIR/RampClk

Could you please give me an explaination why it doesn't work?