This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: EVM bring up and setting question

Part Number: LMK03318

Tool/software:

Hi Team

my customer side meet some question about bring up LMK03318EVM

could you help me check any setup as below is wrong?

1.EEPROM writing issue.

we follow below step to write EEPROM 1a>>2>>3,Read All EEPROM >>GUI map,DATA indicate 0

but EVB doesn't have output and crystal doesn't oscillate. VDD = 3.28V, VDDO = 1.81V, PDN = 2.57V

below is setting file

OLS_20250721.tcs

I2C address also weird.GPIO 1 H=0x7F, MID = 0x7D, L = 0x7C soft ware version is v1.7.9.1

below is current set up for EVM

BRs

Brian

  • Brian,

    Do you have time this week for a live debug? This may be the fastest way to determine the solution. This will likely require reprogramming the EEPROM.

    Is the setting file before or after writing the device? I notice that the I2C address is listed as 0x7F in the header of the file.

    Thanks,

    Kadeem