Part Number: LMK04832
Tool/software:
Hello,
I am trying to generate SYSREF with an LMK04832.
I want to output SYSREF continuously in the same way I did previously with an evaluation board, with a 1.22MHz frequency and 50% duty cycle.
However, with the settings below, SYSREF is only outputting as a 5ns pulse at 2.44MHz. What should I do?
The SYNC is connected to the FPGA but I'm keeping it at a fixed L output. Additionally, I'm configuring the LMK via SPI communication from the FPGA with a 200KHz SCLK, and I can read and write normally.

0x000080
0x000080
0x000200
0x000306
0x0004D1
0x000563
0x000670
0x000C51
0x000D04
0x010002
0x01010A
0x010280
0x010350
0x010410
0x010500
0x010600
0x010700
0x010804
0x01090A
0x010A80
0x010B50
0x010C10
0x010D00
0x010E00
0x010F00
0x011008
0x01110A
0x011280
0x011350
0x011410
0x011500
0x011600
0x011700
0x011808
0x01190A
0x011A80
0x011B50
0x011C10
0x011D00
0x011E00
0x011F00
0x012008
0x01210A
0x012210
0x012350
0x012420
0x012504
0x012600
0x012710
0x012808
0x01290A
0x012A10
0x012B50
0x012C22
0x012D04
0x012E00
0x012F10
0x013002
0x01310A
0x013210
0x013350
0x013420
0x013504
0x013600
0x013710
0x013840
0x013900
0x013A00
0x013B01
0x013C00
0x013D08
0x013E03
0x013F80
0x0140F2
0x014100
0x014200
0x014300
0x0144FF
0x014520
0x014618
0x014710
0x014802
0x014902
0x014A03
0x014B06
0x014C00
0x014D00
0x014E00
0x014F7F
0x015000
0x015102
0x015200
0x015300
0x015478
0x015500
0x015696
0x015700
0x015896
0x015900
0x015A05
0x015BD4
0x015C20
0x015D00
0x015E1E
0x015F0B
0x016000
0x016102
0x016241
0x017360
0x016958
0x016A20
0x016B00
0x016E16
0x017700
0x018200
0x018300
0x018480
0x018500
0x018800
0x016300
0x016400
0x01650C
0x016600
0x016700
0x01680C
0x055500
I found a similar forum thread, but it didn't lead to a solution.
Thanks.