Part Number: LMK04832
Other Parts Discussed in Thread: LMX2594
Hi everyone,
I need to configure the sysref of LMK04832 to work with multi tile in an AMD RFSOC.
My board is HTG-ZRF16 of Hitech with 1x LMK04832 and 4x LMX2594.
The frequency of Sysref is 8Mhz, continuous, in clk10 and clk12, for PL_SYSREF and SYSREF_IN of my RFOSC.
I have this configuration:


After the configuration I progam this sequence:
SYSREF_CLR=1
SYNC_DISSYSREF=0 and SYNC_DISx=0
SYNC_POL=1 -> SYNC_POL=0
SYNC_DISSYSREF=1 and SYNC_DISx=1
SYSREF_CLR=0
SYSREF_MUX=0x03
Do I have a right cofiguration? My RFSOC detects 8Mhz and when I try the DAC outputs of a tile I don't have phase shift with 20Mhz sinusoidal signal but if I have a little phase shift for 190Mhz, a few ps.
Between tiles the phase shift is much greater and it doesn't work the sinchronization.
I don't know if it's a issue of LMK04832 or RFOSC so I would like to know if my LMK configuration is ok.
Thank you in advance.