This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208: Regarding CDCM6208 Clock Generator Suitability

Part Number: CDCM6208
Other Parts Discussed in Thread: TX08D, AFE5809, LMK61E2, LMK5B12204, CLOCK-TREE-ARCHITECT

Hello TI Team,

I have reviewed the CDCM6208 clock generator datasheet and found its performance specifications to be very promising. However, I would like some clarification before finalizing it for our design.

In our application, we are planning to use this clock source for TX08D, AFE5809, and an FPGA. Could you please confirm whether the CDCM6208 is suitable for driving these devices simultaneously, particularly in terms of jitter performance, output format compatibility, and overall system requirements?

I would appreciate your guidance and recommendation on whether this device meets our requirements or if you suggest any alternative solution.

Best Regards,
Harsh Shirke

  • Hi Shirke,

    Please share the requirements of these devices so that we can comment on that. 

    Alternatively you can comment on the Data Converters forum to gain information on their requirements. 

    Best,

    Sandra 

  • Hi Sandra,
    Thank you for your response.


    We are currently designing an 8-channel ultrasound device prototype and require an ultra-low-power, low-jitter clock generator capable of driving all necessary clocks for our modules from a single source. The primary components in our design are the AFE5809, TX08D, and FPGA.


    We would like to confirm whether the CDCM6208 has the capability to provide the required clock signals for all these modules from a single source.


    I have already submitted a support request on the Data Converters forum but have not yet received a response. For your reference, I have included the link to the forum ticket below: AFE5809: Clarification Required on ADC Clock Configuration for AFE5809 Ultrasound Prototype 


    Could you please review our requirements and advise on a suitable solution?


    Best regards,
    Harsh

  • Hi Harsh,

    Thanks for the added information, we have a full clock tree for medical ultrasound front end unit listed in this app note that you can share with the customer 

    https://www.ti.com/lit/an/snaa311a/snaa311a.pdf

    Additionally for the back end unit my understanding is that they need PCIe clocking which they can use the LMKDBxxxx family. 

    Let me know if there are any additional questions

    Best,

    Sandra 

  • Dear Sandra,

    Thank you for your response.

    Within the LMKDBxxxx family, could you please assist us in designing a clock generator circuit that meets our requirements?

    For the AFE5809, we have decided to operate in TGC mode rather than CW mode. Based on this configuration, we would appreciate your guidance in generating suitable clock signals for the AFE5809, TX08D, and the FPGA.

    Best regards,

    Harsh

  • HI Harsh,

     The LMKDBxxxx is a PCIe buffer family.

    The app note I have shared earlier highlights the clock tree based on the requirements of front end unit for ultrasound.  

    As i am not familiar with the requirements of these devices, you will have to share with me the clock requirements (number of channels and their respective frequencies and output formats, jitter requirements and phase noise requirements) so that I can recommend a clock tree 

    Best,

    Sandra  

  • Hi Sandra,

    Thank you for your clarification regarding the LMKDBxxxx PCIe buffer family.

    We are designing an 8-channel ultrasound system, and the clock requirements for the front-end devices are as follows:


    1. AFE5809 (8-Channel ADC Front End)

    • Number of Devices: 1 (8 receive channels)

    • ADC Sampling Clock: 10 MHz to 65 MHz

    • Clock Input Type: LVDS differential preferred

    • Jitter Requirement: < 1 ps RMS (to maintain ADC SNR performance)

    • Phase Noise: Low close-in phase noise required for imaging quality


    2. TX08D (Transmit Section)

    • Clock Type: LVDS differential

    • Frequency: Up to 250 MHz (maximum)

    • Jitter Requirement: Low jitter for precise transmit timing alignment


    3. Cyclone 5E FPGA

    • System Clock: 50–100 MHz (flexible)

    • Reference Clock: Clean differential clock preferred for PLL stability

    • Jitter Requirement: Low jitter recommended for reliable LVDS data capture

    Based on the above requirements, kindly recommend a suitable clock tree architecture for this 8-channel ultrasound system.

    Best regards,
    Harsh Shirke

  • Hi Harsh,

    I'll get back to you by the end of the week 

    Best,

    Sandra 

  • Hi Harsh,

    Apologies for the delay in our response. Based on our understanding of your system, here is a clock tree proposal that I made using this app note. This is for a more traditional ultrasound system, so I've included an additional clock tree below in case you'd like to utilize DPLL advantages as well (i.e. hitless switching, holdover, ZDM).

    The traditional ultrasound clock tree includes fewer clocking sockets and is JESD204B compliant; however, the tree with the LMK5B12204 has the additional advantages of a DPLL, but requires a buffer to fanout the outputs to the AFE. The LMK61E2 oscillator also works well for your application since it is a quartz-based oscillator which has better close-in phase noise.

    The above designs also assume that the frequencies from all 3 devices come from the same frequency domain. More details on the specific frequency plan you plan on using for this application would be needed to further fine-tune this clock tree. Also for your information, here is a link to TI's Clock Tree Architect tool if you'd like an additional source to help with your clock tree architecture.

    Best,
    Jaryd

  • Here's the clock tree architect tool - https://webench.ti.com/clock-tree-architect/