Part Number: CDCE6214
Hi,
I am using a single-ended clock with cliiped sinewave to feed to CDCE6214 reference clock input.
Since the sinewave is only 0.8Vpp, I set the CDCE6214's Reference Input Selection to "Differential Buffer enabled". Is the register setting correct?
I connect the clock input with 100nF coupling cap.
25MHz --------||----------PRIREF_P (pin5)
GND-----------||-----------PRIREF_N (pin6)