Now, I use LMK02000 chip and have met some problem. when I only enable CLKOUT0, the output of the CLKOUT0 is right and the divider and delay time about the CLKOUT0 is correct. but when I enable some other clock-x output.,all the anable outputs are not work and some output signals are DC signal with 1.6V, and some is about 0V,what reasons can cause this problem?
There is another priblem, when LMK02000 is going to lock the reference clock, the frequency of VCXO deviates from the reference clock suddenly and the deviation of the frequency is a little big, that is why? what reason maybe cause the frequency of VCXO changing quickly whe LMK02000 is close to lock the reference clock?
I also find a problem about datasheet of the LMK02000, The chip of LMK02000 used is the national semiconductor corpotation, I find the datasheet released in 2006 and datasheet released have some differences about the control rigister-R0,R14,R15,and this three registers are very improtant for using the chip. how to fiind the differences of LMK02000 chip about the two kind of datasheets?