This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
In the state equipped with CDCE706 to the board that I have designed, you want to write in the EEPROM of CDCE706 using ClockPro.
exp) PC(ClockPro)USB --> CDCE706(on board writing)
When my select the CDCE706 in ClockPro tool, my can select the interface only parallel port.
We want to select the USB, but can not be the case of CDCE706.
Parallel port does not come with my PC.
USB port is attached. Via USB using the ClockPro tool you have installed on your PC,
please tell me how to write to the EEPROM of CDCE706.
Best regards
-----------------------------------------------------------------------
The following texts should be disregarded.
It is the error of Editer. (TPA2006D1)
Hello cafain,
please save your configuration as an Intel HEX file using the CDCE706. Then use the programming EVM to program this file into a device.
Best regards,
Patrick