This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How do I connect a non-crystal clock input to a CC2630?

Other Parts Discussed in Thread: CC2630

There are two pins to connect to a 24MHz crystal oscillator, but I want to use a VCTCXO with a single clock output for the CC2630 clock input. Can I connect this to one of the two crystal pins (X24M_N or X24M_P)?

For example, see section 4.11.3.4 on this datasheet: http://www.ti.com/product/CC3200/datasheet/specifications

Thanks,

Ben