Other Parts Discussed in Thread: CDCM6208, TUSB3410
The first few times I pluged my board to my computer through USB cable after having installed the GUI software, 'DEVICE COMM' and 'PLL LOCK' LEDs were illuminated, as well as the 'PLL Lock' and 'USB Connected' indicators on the GUI. I could change frequency options and all of that on the software.
Then I figured out that when I unpluged my board, my frequencies configuration did not remain.
What I understood was that I needed to use the EEPROM to load my program into the board. I had to install TUSB EEPROM Burner and tried to install different drivers.
Since then, when my board is connected to my computer, the on-board 'DEVICE COMM' and 'PLL LOCK' LEDs are NOT illuminated but the GUI 'PLL Lock' and 'USB Connected' DO are. Also, I can 'Read All' the registers of the CDCM6208 and every single bit is set to '0' except the bit 0 of the register 0.
In summary, I can't find any clear explanations on how to properly load a configuration into my board and I would like to get some help.
Thanks,
Simon