Other Parts Discussed in Thread: CDCE62005
We have two boards, each with a CDCE62005, fed by a single 250MHz CLK, and we want to ensure the outputs of both CDCE62005's are in sync. It seems this question has come up before in this post: https://e2e.ti.com/support/clocks/f/48/t/48547 , however, it is unanswered.
If we use the CDCE62005 basically as a buffer, with the output at 250MHz, how does the PLL lock time affect this synchronization? And the propagation delay that is specified. Will either the PLL lock time or the Propagation Delay change each time the board is powered-ON, or will these times remain constant?
Finally, the first post referenced suggested Fig 32 page 54 in the datasheet, but I do not see this reference in the datasheet - has it been deleted or moved?
~Leonard