hi ,
In order to sdi output synchronous the sdi in , used to the sdi in (rx_usrclk) is the input clock for lmk03200 .The output CLKOUT5 of lmk03200 is used as the reference clock for SDI TX(FPGA GTX REFCLK),now the output clock of lmk03200 has locked the input clock.but sdi tx sent the data is chaotic.If a 148.5mhz crystal is used as the reference clock for the SDI output, the SDI output data is correct.
LMK03200 can be used for SDI applications??
thanks!!!!