This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03328EVM: About output format setting on Code-Loader

Guru 11170 points

Part Number: LMK03328EVM
Other Parts Discussed in Thread: LMK03328

Hi,

I setting work for registers of LMK03328.
Please let me know that how to set output for LVDS format on Code-Loader.

Regards,
ACGUY

set for LVDS format.pdf

  • Hi,

    Auto Mute and Mute Level (controls 1,3) configure Auto Mute, which disables output clock if PLL loses lock. Mute Level sets the voltage the output is pulled to when PLL loses lock (in this case, Vcm).

    Setting 2 configures the output type: DIFF, CMOS, HCSL, or Disable. When choosing one of these options, the other controls functionality changes as well to match this field. In this example, since DIFF is selected, you can ignore the other fields (CMOS, HCSL) which I crossed out.

    The output control 4 is already set to LVDS so no change is needed. Control 5 doesn't do anything in this case since it only applies to HCSL and CMOS. I recommend setting it to HCSL(ExtTerm), same as the control for OUT1.

    Regards,

    -Tim