Other Parts Discussed in Thread: , CODELOADER, USB2ANY, LMX2594, LMX2572
Hello,
I have a question about stepping the frequency in 0-Delay mode using TICS-Pro. I am operating it with the following setup:
Device;LMX2581
Evaluation board: LMX2581EVM in original configuration with internal VCO.
Software; Codeloader program version 4.20.02, Part file version 2014-11-09
Reference; 100MHz
Windows 7 SP1 64 bit
Connected with USB2ANY
Register map (for 0-Delay mode):
R15 0x021FE80F
R13 0x4082410D
R10 0x210050CA
R9 0x03C7C039
R8 0x207DDBF8
R7 0x00082317
R6 0x000004C6
R5 0x0030AC05
R4 0x00000004
R3 0x2004F3E3
R2 0x0C000642
R1 0xC2002021
R0 0x700C0000
When I step the frequency using the N divider (PLL_N) from 600MHz to 650MHz in 0 Delay mode in TICS-Pro, I find the output frequency doesn’t step to 650MHz as expected but only to 602.597MHz. I am stepping N from 12 to 13, and have the divider set at 4.
I discovered the only way I can get an accurate step in frequency I need to follow the following procedure:
- Reprogram the synthesiser with saved non 0-Delay mode register map.
- Change the frequency to what I want in non 0-Delay mode.
- Follow the instructions in 8.3.10 in the LMX2581 datasheet to get to 0-Delay mode again.
Are we meant to be able to step it in 0-Delay mode like I first tried? Is there an easier way to get an accurate step? Or is there something I was doing wrong with the software?
Many thanks!