This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04033: LMK04033

Part Number: LMK04033
Other Parts Discussed in Thread: CODELOADER

I have LMK04033. Pins CLKin drives by 100 MHz. I'm using implementation with crystal oscillator 16 MHz according Figure 16 of datasheet. There are valid signals on pins CLKout0, CLKout2 and CLKout4, but there are no signals on pins CLKout1 and CLKout3. I observe on pin LD that both of PLLs are locked.

Registers values from CodeLoader view:

R7  0x00000017
R0  0x01030A00
R1  0x010B0501
R2  0x010B0502
R3  0x010B0503
R4  0x01030A04
R7  0x00000007
R10 0x2150000A
R11 0x006503CB
R12 0xB019004C
R13 0x0A24000D
R14 0x0217001E
R15 0x1C8003CF

How can i solve my problem withs missing signal on pins CLKout1 and CLKout3?