Part Number: CDCI6214EVM
Any time I attempt to program the CDCI6214EVM using TCIS-Pro SW I will receive "Error while writing into register RX" messages for whatever register the software happens to be writing into at the time. When I instruct the software to "write all registers" this happens for registers R0 to R71, which I am going to assume is all of them. Is there any reason why this might be happening. TCIS-Pro still detects the board and I can still switch the board power through TCIS-Pro, so its obviously successfully communicating with the board.
Prior to observing this problem, I did reconfigure the evaluation boards resistors for a LVCMOS input. I am not certain if this is the cause or I just had not noticed the error messages before.
Thanks for the help.