Hi team,
By setting TCFE=1 for increased charge voltage. Follow all charging guidelines specific to the rechargeable battery or super capacitor when enabling trickle charge.
Not very understand for above description.
The battery is 3V Li-on battery but VCC is 3.3V.
So TCFE=1 will charge the battery up to VCC voltage, right?
That means need to external sense battery voltage when at 3V and then set TCFE=0?
Or trickle charger function is not suitable for 3V battery?
Thank you!