This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Experts,
I would like to use LMX2572 to design frequency hopping system with 1000 hops in one second.
I know I can trigger Muxout pin to monitor VCO Cal Time, and the window of VCO Cal signal is total VCO calibration time.
If I set frequency A hop to frequency B,
How do I know the exactly time that the signal is disappear on frequency A and appear on frequency B ?
Thanks a lot.
Derek
Hi Derek,
Our expert on this series of products, Dean, is on vacation until Sep 4. Dean didn't leave much documentation on 2572, so please refer to the following notes on 2594 and see if it helps:7651.Fast frequency switching full assist.pdf
Regards,
Hao