Part Number: TLC555
Other Parts Discussed in Thread: SN74LVC1GX04
Hello,
I have a really basic question.
I designed an Astable 555 timer circuit with an output frequency of 100kHz.
However, even though I set its output frequency to 100kHz by varying the resistors, it never remains fixed and changes by 4-5% during operation.
I thought that the problem was with the timing capacitors I was using. So I replaced them with class I ceramic caps. But still, I have the same issue.
Even after i reset the TLC555 IC it continues to operate at the wrong frequency.
Can someone please guide me to what can the possible error?
or can suggest some new circuit with a more robust output.
-Ankit