Part Number: LMX2594
Dean,
Is there a specification in the LMX2594 data sheet that determines the minimum input clock jitter or precision above which the device is not able to achieve phase SYNC or lock? I.e. percent of clock period or ppm, etc. I ask this because we are attempting to lock to an intermediate PLL-based device which conforms to the following JEDEC Standard No. 82-31, Table 83 attached below. So far, we are able to successfully lock to the 1.2GHz input clock to this device, but not to its output clock with the specifications in Table 83. I'm suspicious that the added jitter is the culprit. If so, can the loop filter be adjusted to accommodate this additional jitter?
Thanks,
- Ken