This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: Resetting the divider and generating sysref

Expert 1585 points
Part Number: LMK04828


Hello 

I want to use LMK04828 in order to achieve two goals: 

1. Divide the input signal by 30 and reset the divider at deterministic timing generating a known phase 100MHz clock

2. Generate SYSREF to DAC38RFxx aligned to DACCLK with the proper setup and hold time. 

In order to do that: 

Fin = 3GHz external input to the part at port Fin, goes to the DACCLK through LMK

One time strobe to sync or sysref input in order to: 

1. Reset the divider by 30 to have the clock 100MHz output at a deterministic phase and timing

2. Align the SYSREF to the DACCLK

Can you please advise what is the required setup? 

What is the alignment mechanism? Does the LMK moves the SYSREF relative to the DACCLK or the opposite? 

Thanks

  • Hello Izik,

    I understand you are distributing a 3 GHz signal through CLKin1/Fin pins to DAC with SYSREF, but also want to divide /30 to generate 100 MHz which has a known phase as defined by an external SYNC.  I'm not sure your SYSREF frequency, but that wouldn't expect it to impact my answer.

    This is possible.  To achieve this you will need to send a SYNC pulse into the CLKin0 input and meet timing to CLKin1 input at 3 GHz.  The period of 3 GHz is is ~333 ps.  I recommend the SYNC pulse to occur on falling edge of 3 GHz input clock to CLKin1.  See attached document for example plots.

    Using LMK04828 as JESD204B Fan-out, 3 GHz setup and hold.pdf

    When giving this SYNC, configure the device such that CLKin0_OUT_MUX = 0 (Drive SYSREF_MUX), SYSREF_MUX = 0 (Normal SYNC), SYSREF_CLKin0_MUX = 0 (SYSREF_MUX).  Now for each divider you want to reset to have deterministic phase, set SYNC_DISX = 0.  Also to ensure SYSREF signal is synchronized, set SYNC_DISSYSREF = 0.  This allows your external SYNC pulse on CLKin0 to reset the dividers.  After the SYNC pulse is given, set all SYNC_DISX/SYSREF bits = 1 so that your SYSREF pulse does't disrupt the output.  Please refer to section 9.3.2 for more details on configuring SYSREF... as SYNC and SYSREF share the same clock path.  Depending on your SYSREF configuration, you will need to re-configure the muxes.

    -

    To achieve timing of SYSREF to DACCLK at DAC input.  I recommend adjusting the digital delay on the SYSREF.  This means keeping device clock fixed and adjusting SYSREF clock.  While the device clock path has 25 ps steps of analog delay, it will increase your noise floor.  While you can do this to get finer timing adjustments, analog delay also has increased variation over PVT vs. digital delay, so depending on DAC frequency, you may need to accommodate for shift over temp.  Note, you could also use the 150 ps step analog delay step in sysref path and the digital delay step in sysref path together such that the difference is 166.5 ps - 150 ps = 16.5 ps.  This gives an effective time adjustment of ~16.5 ps.  It will actually very as the analog delay steps are not perfectly 150 ps.  Also, as above, there will be analog delay sensitivities with respect to PVT you may need to accommodate for.  Normally digital delay is sufficient to meet setup and hold times.

    73,
    Timothy

  • Dear Timothy

    Thank you for your prompt and detailed answer.
    I want to focus on the timing requirements between the sync signal and the actual divider reset and the sysref output event timing.
    I need to have deterministic latency between the sync and the actual divider reset and the sysref, between sync events, and also between repeated on/off cycles to the LMK part.

    It means that for example, if the div. reset occurs 200 nS after the rise of the sync, it has to be the same constant number between repeated sync events and also remain 200nS between power-up cycles.

    I understand that in order to achieve that, we need to make sure that the sync meets the setup and hold of the high frequency (3GHz) DACCLK. this was the nature of the slides that you sent. Is that correct?

    Unfortunately, in my system, the sync is asynchronous to the 3GHZ DACCLK. Does that means that I will have +/- 1 DACCLK uncertainty in the divider reset and the sysref output? Can you offer a solution for this problem?

    Many thanks
    Izik
  • Hello Izik,

    If I could come up with a solution, I think I need more info.

    Is your SYSREF 100 MHz?

    Do you have multiple LMK04828 you want synchronized together from an asynchronous request?

    Do want the LMK04828 SYSREF aligned  with some other low frequency associated with your asynchronous request?
          * If so can you advise what frequency it is?  That is the lowest frequency to which you need determinism and a slip of one cycle is transparent?  Perhaps the SYSREF frequency?

    Note from JESD204B requirements.  JESD204B does not care if when you issue the SYSREF pulse provided time_of_SYSREF modulus Local_Multi_Frame_Clock_period = 0.  Your application may (or may not) care if this time is the same.  JESD204B has deterministic timing only within the LMFC period.  Beyond that you must keep track of things.

    By definition, the SYSREF period is equal to some integer multiple of LMFC period.  Therefore SYSREF_period modulus Local_Multi_Frame_Clock_period = 0.

    Izik said:
    It means that for example, if the div. reset occurs 200 nS after the rise of the sync, it has to be the same constant number between repeated sync events and also remain 200nS between power-up cycles.

    It would, provided the input conditions are met... except by definition of the asynchronous SYNC request, the time will not be strictly the same.  In an ideal/theoretical system the timing will vary from 0 seconds to just less than 1 DACCLK period due to asynchronous nature of your input.  Is uncertainty of SYNC to SYSREF of +/- 1 (or 0 to 2 cycles) that much worse for your system?

    73,
    Timothy