This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bidirectional buffer with Better VOH and VOL

Hi,

Buffer need to be placed between below two ICs. their noise margin levels are in negative. Please suggest me the bidirectional auto detection buffer or  level translator with which works on the below condition.

In my case, margin levels are,

Input IC's Vih min = 1.44V. 
output IC's Vohh min= 1.40V and

input IC's Vil max= 0.36V

output IC's Vol max = 0.4V.

Thanks,

Vignesh.