Hi Timothy,
Following up on this question from a while back.
I'm currently trying to figure out how to achieve a 0-delay scheme with my LMK04828B system. You suggested supplying a reference that was equal to my SYSREF frequency and I have a few follow up questions.
- What is the difference between the two 0-delay modes? (Cascaded vs Nested). It seems in nested mode, the VCXO will not be deterministic to the CLKin or CLKouts, Why would this mode be used over cascaded?
- Is it possible to adjust the "K" parameter in JESD204B such that my SYSREF frequency is equal to my OSCin reference frequency? The XO operates at 122.88 MHz. With an LMFS = 2441, and a sampling rate of 245.76 MSPS, if I choose K = 2, I could achieve a maximum SYSREF frequency of 122.88 MHz. This would thus allow me to use my current hardware for 0-delay mode.
- Finally, in 0-delay mode it seems that there are a few options for reference in feedback - SYSREF, CLKout6, CLKout8, and External. I currently have an unused CLKout6 - could I configure these dividers to generate a 122.88 MHz clock, use it as feedback in 0-delay mode, and achieve deterministic phase relationships for my CLKins and CLKouts?
Thanks!
Eldrick