This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: Lock detect R110 intermittently reports unlocked when PLL is locked

Part Number: LMX2595

The lock detect value reported in R110 sometimes reports unlocked even though the PLL is locked.

I have only see this for certain frequencies and when using the reference doubler with a 200 MHz PFD.

I tuned the LMX2595 from 8000 to 15000 MHz (10 MHz steps) and recorded the lock detect value from R110. I did this using 100 and 200 MHz PFDs.  For the 100 MHz PFD, I used a fractional denominator of 10.  For the 200 MHz PFD, I used a fractional denominator of 20.  The plot below shows the results of this test.

Any idea why this happens?

FYI - The MUXout pin always reports lock detect consistent with the PLL being locked.