Part Number: LMX2595
Respected sir/madam.
I am developing a frequency synthesizer to generate 17GHz with a bandwidth of 200MHz. After loading the design in TICS pro software as per our requirement and obtaining all the register values we need to load this register values in the controller in order to fabricate it on PCB. As per the evaluation board the values of the registers are directly loaded into the controller and there is no need of programming. But in order to fabricate we need to load in controller. Can anyone suggest me in selection of the controller and how do I interface that controller with LMX2595 IC and any source code for programming.
Thanks in advance