Part Number: CDCE925
Other Parts Discussed in Thread: CDCE913, , CDCE937, CDCE949
Hello,
I am trying to understand the addressing scheme for CDCE925 / CDCE913.
If I have a CDCE925 and CDCE913 on the same I2C bus, how do I take advantage of the A1 / A0 bits?
It looks like, from the data sheet, that the top 5 bits of the CDCE913 and CDCE925 address bits are the same, so if you can change the lower two bits you could potentially make the CDCE913 and CDCE925 the same address - making it impossible to distinguish between the two. Likewise, the CDCE937 and CDCE949 share the same top 5 address bits yet appear to have the bottom 2 address bits be programmable.
It also looks like the addresses given are the default ones which does make them unique.
Is it intended that the A1 / A0 bits are programmed outside the system, off the PCB, if the system has more than one CDCE chip?
An explanation of how the A1 / A0 bits are intended to be used would be most appreciated.