Part Number: CDCE62002
In the EVM, choosing LVDS input buffer, sets INBUFSELX = 1, and INBUFSELY = 0. The data sheet indicates that in order to select LVDS on the input, it should be (X,Y) = (01).
Either the EVM is in error or the data sheet. Which one is correct? I am leaning towards the data sheet being correct because there is a note in the Revision history that bits 0 and 1 were corrected.
Also, it is very confusing when some parameters in the data sheet are listed with LSB to the right and others are listed MSB to the right. All the input and output buffer select bits are listed MSB to the right, as are the smart mux bits, all other parameters are LSB to the right as shown in the Tables.
There are many bits in register two that are listed as reserved or for TI use only. However, the data sheet does not indicate what should be written to these bits when writing to register two. I have been setting those bits to zero, is this correct?
One last comment. The EVM software has a button for EEPROM Write, and another for EEPROM Write + Lock. The data sheet shows in the revision history that references to EEPROM Locking has been removed. Is this feature no longer available? In any case, I have not been able to get the EEPROM feature to work at all, which is not a big deal because I do not need.
Thanks
Jerry Ethridge
Sr Hardware Engineer
AMX by Harman - Dallas
3000 Research Drive
Richardson, TX 75082
Phone: 469.624.7611